1. The 'S32V234 Treerunner external.pdml' file is a Flotherm assembly file. It is not a project file. 
2. The file must be imported as an assembly under the root folder of an existing Flotherm project file.
3. The power value attached to the die need to be modified in accordance with the product's application power scenario.